AXIS#.MOTOR.TEMPC

Description

When the motor has a thermistor with linear characteristics (AXIS#.MOTOR.RTYPE = 2, 3, 4, or 8), AXIS#.MOTOR.TEMPC returns the motor temperature in degrees Celsius, which is calculated from the resistance of the motor thermistor.

There is no algorithm to convert from resistance to degrees Celsius for non-linear thermistors. In this case, AXIS#.MOTOR.TEMPC returns -32,768 which is an invalid temperature.

Context

For more information see Motor and Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Degrees Celsius

Range

-215 to 215
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
AXIS1.MOTOR.TEMPC

500bh

01h

Signed16

-

-

Read only

Yes

AXIS2.MOTOR.TEMPC

510bh

01h

Signed16

-

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TEMPC

6235

185B

Signed16

Read Only

-

AXIS2.MOTOR.TEMPC

71771

1185

Signed16

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TEMPC

6235

Signed16

Read Only

-